I use an LCD with a pixel clock of 33MHz. I set my source to pll5 in clk-imx6q.c to allow a clock lower than 38MHz.
I also display a logo from the kernel.
However, during the logo display, the pixel clock measure approx. 8MHz.
After the kernel boots, the pixel clock is 33MHz as desired.
How can I correct the initial pixel clock?
I am using an iMX6q, Linux 3.10.
Hi Dave
please look at patches provided on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------