Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or cancel? BR Max Ariza
Hi Manuel,
The Data_In pin of the receiver board is pulled HIGH to 5V to disable TX in receiver.
This can be confirmed in UM10422 for the TDA5051A demo boards, see transmission test setup in Table 3 of this document: https://www.nxp.com/docs/en/user-guide/UM10422.pdf
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jose
Thanks for you support !
Best regards
Max Ariza
Field Application Engineer
Manager
PLEASE NOTE, MY EMAIL ADDRESS HAS CHANGED
Arrow Components México, S.A. de C.V.
Mobile2 +52 1 55 1885 9330
Mobile2 +52 1 656 130 9261
www.arrow.com<http://www.arrow.com/>;
De: reyes
Enviado el: miércoles, 20 de septiembre de 2017 11:24 a.m.
Para: MANUEL Ariza <maximiliano.ariza@arrow.com>; MANUEL Ariza <maximiliano.ariza@arrow.com>
Asunto: Re: - Re: Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or canc...
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or cancel?
reply from Jose Alberto Reyes Morales<https://community.nxp.com/people/reyes?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/945016?commentID=945016&et=watches.email.thread#comment-945016>