Hi All:
I am using Firefox as my browser with x11.
I build firefox with this command `bitbake firefox`.
It all fine during the compiling.
But here is the problem when I execute firefox in my rootfs.
Here is the error that I got:
XPCOMGlueLoad error for file /usr/lib/firefox-38.4/libxul.so:
libvpx.so.2: Cannot open shared object file: No such file or directory
Couldn't load XPCOM.
When I check the library that yocto project built out and found no libvpx.so.2.
How to solve this question?
Thanks in Advanced.
Hi Wang
for firefox one can check boundary devices releases:
Morty Yocto Release i.MX6 Series - NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------