OMNIVISION OV5640 5MP AF module with MIPI interface on phyCORE-i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OMNIVISION OV5640 5MP AF module with MIPI interface on phyCORE-i.MX7D

701 Views
nagamaheshg
Contributor III

We are working on our custom carrier board with  phyCORE-i.MX7D SOM.
Now we are trying to interface OMNIVISION OV5640 5MP AF module which has MIPI interface on phyCORE-i.MX7D.

Does this camera works with phyCORE-i.MX7D, please  share your comments.
How to integrate this camera successfully with phyCORE-i.MX7D.

Labels (1)
0 Kudos
1 Reply

517 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nagamahesh

seems this is possible as its BSP is based on NXP Release L4.1.15-2.0.1_ga, according to

BSP Yocto FSL iMX7 PD17.1.0 Release Notes - Develop.phytec - PHYTEC Wiki  

and one can follow Chapter 19 OmniVision Camera Driver attached Linux Manual.

Since this is third party board, it is supported by its vendor, issue may be posted on

http://support.phytec.com/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos