AnsweredAssumed Answered

Send text data to a specific Zigbee Node with HA (NXP Zigbee HA)

Question asked by dostshah on Sep 6, 2017
Latest reply on Sep 13, 2017 by David Ashraf

I have a Zigbee End-device based on JN5168, I want to realize it as a lock that is battery powered. Apart from accepting the HA lock cluster commands, I need to send some custom data (some text as commands) for extra features that I want to add to the system. How can I send such data and receive it at lock? Do I have to implement a custom cluster along or is there another way?

Outcomes