Hi,
Some patchs was released, for i.MX6 IPU and rotating a frame buffer for kernel 3.10.17 and it was ok.
unfortunately, the new kernel version 4.1.15 is not compatible with the existings patchs.
I am try to adapt the existing patch for the 4.1.15 kernel version but it is too hard for me.
Please anybody can help me ?
May be a person can adapt the existing patch to obtain a rotoating frame buffer.
Thanks in advance
Franck
Hello Franck,
Can you please tell me which patches are you applying?
Best Regards,
Diego.
HI Diego,
I do not find any patches for the kernel version 4.1.15
The patches that I have found, was for the kernel 3.10 but there are not compatible with the new kernel versions.
Best Regards
Franck
De : diegoadrian
Envoyé : mercredi 13 septembre 2017 23:33
À : FRANCK HANSEN
Objet : Re: - Re: i.MX6 IPU and rotating a frame buffer for kernel 4.1.15
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: i.MX6 IPU and rotating a frame buffer for kernel 4.1.15
reply from Diego Adrian Cuevas <https://community.nxp.com/people/diegoadrian?et=watches.email.thread> in i.MX Community - View the full discussion <https://community.nxp.com/message/942818?commentID=942818&et=watches.email.thread#comment-942818>