I'm using i.MX6 q4 OTG, system: linux, kernel version: 3.0.35 .
I found a problem that the OTG host mode can not be identified after the device boot up;
when booting the linux kernel , I insert the Micro USB cable(let the ID pin level low) the OTG host mode can be idenfied correctly;
Hi Sharp
one can check if usb_id signal is grouned and test with unit
tests package (folder /mxc_usb_test)
Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------