I've made a binary file(*.bin) using another compiler which is compatible with the GNU, but when using the PEMICRO-jtag to download the binary into the mpc5674f's internal flash ,the tool doesn't allow me to do so by using the "DATA_LOAD" command ,I don't know what's wrong with it. I would appreciate it if anyone can explain the reason or offer me some other ways to program the binary file into the mcu's internal flash.
NOTE: not an elf because the tool is ok with the codewarrior's elf output file.
Or you can contact me through my email :270893779@qq.com .
Hello,
I think this is question for PEMicro. Could you please contact their support? They should be able to provide you more accurate information.
Regards,
Martin