Hello,
You can use the $ifconfig command to configure the network just as it is shown in the following image.
If you want to do it in the code, you can do it by using the bind address function:
IP_IF_BindAddr6(ifHandle->ifUniqueId, &inIpAddr,ip6AddrTypeManual_c,
IP6_ADDRESS_LIFETIME_INFINITE, 64U);
Best Regards,
Estephania
Hi Estephania,
This is perfect.
Thank you!
Kind regards.
Fabrice
2017-09-12 6:46 GMT+02:00 estephania_martinez <admin@community.nxp.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: How to set a fix IPv6 to Thread leader
reply from Estephania Martinez Garcia
<https://community.nxp.com/people/estephania_martinez?et=watches.email.thread>
in Kinetis Software Development Kit - View the full discussion
<https://community.nxp.com/message/941925?commentID=941925&et=watches.email.thread#comment-941925>