CAN Master and slave testing on S32K144 EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Master and slave testing on S32K144 EVB

1,190 Views
mrajanna
Contributor V

Hi,

I am testing CAN Master and CAN slave on two different S32K144 EVB.

It seems transmit and receive is not working.

Test Setup:

Below picture shows the test setup.

pastedImage_4.png

 

I have connected two different S32K144 EVB's to two PC and running separate master,slave debug sessions.

Please guide me the exact steps to test CAN_MASTER and CAN_SLAVE sample examples with pictures if possible.

Awaiting for the response. 

Thanks

Mohan 

Labels (1)
Tags (2)
0 Kudos
3 Replies

780 Views
AnaAldescu
NXP Employee
NXP Employee

Hello,

This example needs a 12V power supply in order to work properly. Please see the example documentation.

Regards,

Ana

780 Views
mrajanna
Contributor V

Thank you Ana.

What is the expected Ampere ? whether 2 Ampere is OK ?

0 Kudos

780 Views
AnaAldescu
NXP Employee
NXP Employee

Yes, 2A should be OK.

Regards,

Ana