Kernel version is 4.1.15,when we select IEEE 802.11 for Host AP(Prism2/2.5/3 and WEP/TKIP/CCMP) in Wireless LAN menuconfig

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel version is 4.1.15,when we select IEEE 802.11 for Host AP(Prism2/2.5/3 and WEP/TKIP/CCMP) in Wireless LAN menuconfig

1,105 Views
youyong
Contributor I

udevd[196]: starting version 3.1.5
random: udevd urandom read with 20 bits of entropy available
galcore: disagrees about version of symbol wake_up_process
galcore: Unknown symbol wake_up_process (err -22)
galcore: disagrees about version of symbol __task_pid_nr_ns
galcore: Unknown symbol __task_pid_nr_ns (err -22)
galcore: disagrees about version of symbol pid_task
galcore: Unknown symbol pid_task (err -22)
galcore: disagrees about version of symbol device_create
galcore: Unknown symbol device_create (err -22)
galcore: disagrees about version of symbol dev_err
galcore: Unknown symbol dev_err (err -22)
mxc_dcic: disagrees about version of symbol device_create
mxc_dcic: Unknown symbol device_create (err -22)
mxc_dcic: disagrees about version of symbol dev_err
mxc_dcic: Unknown symbol dev_err (err -22)
mxc_dcic: disagrees about version of symbol device_destroy
mxc_dcic: Unknown symbol device_destroy (err -22)
mxc_dcic: disagrees about version of symbol device_create
mxc_dcic: Unknown symbol device_create (err -22)
galcore: disagrees about version of symbol device_destroy
galcore: Unknown symbol device_destroy (err -22)
galcore: disagrees about version of symbol find_vpid
galcore: Unknown symbol find_vpid (err -22)
galcore: disagrees about version of symbol pid_vnr
galcore: Unknown symbol pid_vnr (err -22)
ov5640_camera_mipi_int: disagrees about version of symbol dev_warn
mxc_dcic: disagrees about version of symbol dev_err
mxc_dcic: Unknown symbol dev_err (err -22)
ov5640_camera_mipi_int: Unknown symbol dev_warn (err -22)
ov5640_camera_mipi_int: disagrees about version of symbol dev_err
ov5640_camera_mipi_int: Unknown symbol dev_err (err -22)
mxc_dcic: disagrees about version of symbol device_destroy
mxc_dcic: Unknown symbol device_destroy (err -22)
galcore: disagrees about version of symbol wake_up_process
galcore: Unknown symbol wake_up_process (err -22)
galcore: disagrees about version of symbol __task_pid_nr_ns
galcore: Unknown symbol __task_pid_nr_ns (err -22)
mxc_v4l2_capture: disagrees about version of symbol device_create_file
mxc_v4l2_capture: Unknown symbol device_create_file (err -22)
galcore: disagrees about version of symbol pid_task
galcore: Unknown symbol pid_task (err -22)
mxc_v4l2_capture: disagrees about version of symbol dev_err
mxc_v4l2_capture: Unknown symbol dev_err (err -22)
galcore: disagrees about version of symbol device_create
galcore: Unknown symbol device_create (err -22)
mxc_v4l2_capture: disagrees about version of symbol device_remove_file
galcore: disagrees about version of symbol dev_err
galcore: Unknown symbol dev_err (err -22)
galcore: disagrees about version of symbol device_destroy
mxc_v4l2_capture: Unknown symbol device_remove_file (err -22)
galcore: Unknown symbol device_destroy (err -22)
mxc_v4l2_capture: disagrees about version of symbol device_create_file
galcore: disagrees about version of symbol find_vpid
galcore: Unknown symbol find_vpid (err -22)
mxc_v4l2_capture: Unknown symbol device_create_file (err -22)
galcore: disagrees about version of symbol pid_vnr
galcore: Unknown symbol pid_vnr (err -22)
mxc_v4l2_capture: disagrees about version of symbol dev_err

Labels (2)
0 Kudos
2 Replies

748 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which BSP are you using?

Which board are you using?

Do you mean all the things back to normal if not select "IEEE 802.11 for Host AP(Prism2/2.5/3 and WEP/TKIP/CCMP)" in menuconfig?

0 Kudos

748 Views
youyong
Contributor I

1、BSP version is 4.1.15-2.0.1+

2、board is iMX6DL sabresd

3、if not select "IEEE 802.11 for Host AP(Prism2/2.5/3 and WEP/TKIP/CCMP" ,it is ok,but can not support "iwlist wlan0 scan"

0 Kudos