How to use PE attach MPC5746C with JTag?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use PE attach MPC5746C with JTag?

694 Views
dududdd
Contributor I

Hi,all

     S32 software prompted : "The target may have entered reset escalation. please power cycle the board."when I used PE attach MPC5746C with JTag. How can I solve this promblem?

     

     best regards!

     Thanks!

Tags (3)
0 Kudos
2 Replies

556 Views
dududdd
Contributor I

When I tried to use LAUTERBACH to connect the board, it showed that debug port fail. And then,I pulled down the RESET PIN of the MPC5746C chip and pulled up the board.Meantimes,I used LAUTERBACH to connect the board. And then,I could debug it.

0 Kudos

556 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

if you are able to connect using Lauterbach debugger, you should be also able to connect using PEMicro debugger. Which PEMicro debug probe you use and which version of S32DS you use?

Could you please send me the measurement of the reset signal after power on reset?

Regards,

Martin

0 Kudos