Can you please provide the file containing the implementations of the generic interrupt
controller handling routines for LS1021A?
Project is compiled and flash file is generated using code warrior.
Look at program example in CodeWarrior folder. For example, use the following path to DUART program example:
C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Serial\Common
This example uses interrupt from DUART.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------