LPC1788 has one LCD controller interface, and used it for AUO 7" LCD (800x480) for quite a time.
Now I'd like to drive a WXGA(1280x800) TFT LCD with LVDS interface. I've select a RGBtoLVDS plane driver. But I'm in doubt whether LPC1788 can afford the high clock required by the WXGA LCD(say, ~68MHz)...
If I use LPC1788 to drive such a display, would it totally cannot work, or just a slow refresh rate?
Solved! Go to Solution.
Hi Jack,
It is not possible for the LPC1788 to drive such a display, the programmable display resolution can be configured up to 1024 × 768 (XGA).
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
OK, thx.
I'll set off to find another controller.
Hi Jack,
It is not possible for the LPC1788 to drive such a display, the programmable display resolution can be configured up to 1024 × 768 (XGA).
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer