Support-
I need to debug a P1010 but it is in a JTAG chain with an MPC5125.
How can I create the correct JTAG config file?
Codewarrior fails due to an unrecognized core.
Is there an option for the 5125 in CW?
should I define it as GENERIC? with what jtag parameters please?
Thank you.
Robert
Hi Robert
I wonder if your question is specifically for having P1010 and MPC5125 on the same chain or finding the right config for MPC5125. Were you able to connect to MPC5125 independently or are you also looking for a config file just to do this ? I thought if you clarify you might get more help here.
Regards
Sinan Akman