Hello
I have a question about the CBTL02043ABQ differential channel mux demux.
I am not sure if this is the correct community for this device. If not, I apologize.
I would like to use this device to switch SGMII high speed serial signals (1.25Gbps). SGMII differential pairs are AC coupled with a common mode voltage of 0V.
I would just like to confirm that this device can handle signals that swing to negative voltages even though it's power rails are only +3V3 and GND. Because the SGMII common mode voltage is at 0V, the signals will swing both positive and negative relative to the 0V common mode.
I can find a maximum input voltage for the differential pins of 2.4V in the datasheet but I cannot find a minimum.
Thank you.
Solved! Go to Solution.
Hello Gavin,
The minimum input voltage at the differential pins is -0.3V.
Regarding “SGMII differential pairs are AC coupled with a common mode voltage of 0V” - as I understand SGMII usually uses LVDS as its I/O, which has a common mode voltage at about 1V-1.3V. Do you use a different flavor I/O?
Best regards,
Tomas
Thank you Tomas. I will make sure my differential signals are biased in the range 1V - 1.3V.
Hello Gavin,
The minimum input voltage at the differential pins is -0.3V.
Regarding “SGMII differential pairs are AC coupled with a common mode voltage of 0V” - as I understand SGMII usually uses LVDS as its I/O, which has a common mode voltage at about 1V-1.3V. Do you use a different flavor I/O?
Best regards,
Tomas