AnsweredAssumed Answered

Debug in SDRAM

Question asked by biafra on Aug 25, 2017
Latest reply on Aug 31, 2017 by biafra

Hi everyone,

 

I posted another question about loading an application to debug in SDRAM in the postDebug in SDRAM using KDS toolchain, referred to summarize the basic steps.

I was forced to switch to IAR toolchain because KDS doesn't allow to load the application code in SDRAM. I'm working on a custom board based on K65FX1M0M18 using J-Link or Multilink Universal debugger.

In the board there are:

  • K65FX1M0M18
  • External SDRAM (4M x 32)
  • External flash (2M x 16),

 

Now I'm considering to switch to MCUXpresso toolchain, but my doubt is the same: does MCUXpresso toolchain allow to load the application code in SDRAM? If so, how can it be done?

 

Many thanks,

Biafra

Outcomes