P2020 Processor usb not detcted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 Processor usb not detcted

765 Views
nareshpuli
Contributor III

Hello,

i am using P2020RDB customized board initially it is worked fine,due to voltage drop we populated ext. 1V to the processor few days latter suddenly  USB port is not working that when i connect.

we have USB3300 ic beween the processor and usb port

 

please what could the the problem for the boot halting, if any one help would be appreciated

Best Regards

Naresh

have a good day !!!!!!!!!

Labels (1)
0 Kudos
3 Replies

542 Views
nareshpuli
Contributor III

hello,

finally i found that issue due to the USB 3300 chip clock issue,it is not fully booted Between the processor and usb port we have one ic(USB3300)

but now it is booting fine.

0 Kudos

542 Views
nareshpuli
Contributor III

Booting fine, but USB port is not detecting any device what could be the problem ??

0 Kudos

542 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello sivakumar puli,

Please go to u-boot prompt, configure the following:

hwconfig=usb1:dr_mode=host,phy_type=ulpi;usb2

Please connect the USB mass storage device and execute the following commands to check whether USB device information can be detected successfully.

=>usb start

=>usb reset

=>usb tree

=>usb info

=>usb storage

=>usb dev


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos