AnsweredAssumed Answered

MK20DX256VMC7 IDD_VBAT when VDD = 0

Question asked by phil74 Employee on Aug 21, 2017
Latest reply on Aug 22, 2017 by EARL GOODRICH

Hello,

 

Can you confirm that the RTC of MK20DX256  can still run on Vbat voltage even if main MCU Vdd = 0 , and then IDD_VBAT average current is Max 0.94µA at 3.0V, –40 to 25°C, according to datasheet?

 

Thanks in advance,

Best Regards,

Philippe

Outcomes