Hai friends , I am new to this microcontroller.I have an doubt regarding FRDM-K64 microcontroller.I have question:1.What is the maximum amount of sensors that I can interface especially in this type of microcontroller? thank u

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hai friends , I am new to this microcontroller.I have an doubt regarding FRDM-K64 microcontroller.I have question:1.What is the maximum amount of sensors that I can interface especially in this type of microcontroller? thank u

273 Views
balajiv
Contributor II

FRDM -K64 MICROCONTROLLER31958-FRDM-K64F_BD.jpg

1 Reply

231 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Balaji V,

It depends on the interface of the sensor, for example, if the sensor has iic interface, you may connect multiple sensors with this MCU via the iic port.

Hope that makes sense,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------