[CW5.2] I want to output a warning message to a file.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[CW5.2] I want to output a warning message to a file.

468 Views
donggiyeom
Contributor I

I want to output a warning message to a file.

-WOutFileOn command was able to output an error message.

However, I can not find an option to print a warning message to a file.

Please tell me.

Tags (2)
0 Kudos
1 Reply

280 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi donggi.

I just checked option -WOutFileOn, it can output warning but it has problem. see my attached testing video.

warning messages can be printed to EDITOUT but it must be after error messages.

I wonder this is the problem of option -WOutFileOn.

Unfortunately there is no other option can utilize this feature.

as a workaround, if you use CW IDE -  I advise doing Ctrl+C when the "Errors & Warning" message window is ACTIVE. Then just do Ctrl+P in a separate file to paste all the errors and warnings.


Have a great day,
Jennie Zhang

-

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------