Hello,
I am working on IMX6Q Board which is similar to sabre-sd. On this board we have eMMC ( 4G ).
For board testing i have partitioned the eMMC with two partitions boot and rootfs.
I have loaded the dtb file and zImage in boot partition and file system in rootfs partition.
Once I powered up the board. i just load the u-boot.imx using imx_usb_loader.
This u boot loads the kernel and it working fine.
But, I would like to store the u-boot also in the eMMC and u-boot must load on power up.
Please do point me to make this happen.
Solved! Go to Solution.
Hi Venkata
please refer to sect.4.4.1.2 Using eMMC attached Linux Guide. Also one can
use mfg tools from link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Venkata
please refer to sect.4.4.1.2 Using eMMC attached Linux Guide. Also one can
use mfg tools from link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------