Hi ,
I am working on imx6 solo custom board with linux yocto. now working on max 17059 fuel guage IC.
its capacity is as follows:
5.5V-0%
7.4V-50%
8.4V-100%
At 8.4V it shows 100% but it shows 0% at 7V only and board will be ON for 3 to 4 hours even after it shows 0% battery.
How can i solve this issue?
Please suggest
Thanks and Regards
Rizwan Syed
Hi Rizwan
one can check sensor ground connections and software with max 17059 evk and software
MAX17059 1-Cell/2-Cell Fuel Gauge with ModelGauge - Maxim
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------