AnsweredAssumed Answered

MPC5668G, interrupt on PA0 pin?

Question asked by SUKRUTH RAMESH BABU on Aug 16, 2017
Latest reply on Aug 23, 2017 by Petr Stancik

Hi,

 

I am trying to install an interrupt on the pin PA0(with the pad number 0).

But interrupt for this pin doesn't seem to be generated.

I have enabled the corresponding pin of IREER , IFEER , DIRER and using the Vector number 53(from the manual)?

Can you please support me by suggesting if I am missing any additional configurations?

Or if available ,Please attach the example code in which PA0  state is used for for generating an interrupt.

 

Regards,

Sukruth  

Outcomes