Does i.MX7 Dual SABRE Board support HDMI output? If yes, where do I find more info regarding this?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX7 Dual SABRE Board support HDMI output? If yes, where do I find more info regarding this?

930 Views
anil_sasidharan
Contributor I

We would like to drive the display output from an i.MX 7Dual SABRE Board onto an HDMI monitor. Is this possible? Can someone please share more details on this.

0 Kudos
3 Replies

631 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Anil,

Yes, you can find documentation in the Supporting Information Section.

i.MX 7Dual SABRE Board|NXP 

The specific information below can be found in the iMX Linux Users Guide.

Boot up the system through RFS in eMMC by HDMI:
• For i.MX 6 boards:
U-Boot > setenv mmcargs 'setenv bootargs ${bootargs} root=/dev/mmcblk3p2 rootwait
rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'
• For i.MX 7Dual SABRE boards:
U-Boot > setenv mmcargs 'setenv bootargs ${bootargs} root=/dev/mmcblk2p2 rootwait
rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

631 Views
anil_sasidharan
Contributor I

Hi Carlos,

Thank you so much for your answer. In fact while going through the data sheet for i.MX7 (IMX7DCEC_iMX7_Dual_data_sheet), I've observed that only 2 types of display interfaces are supported, Parallel RGB and MIPI-DSI. Whereas the i.MX7 Dual SABRE Board claims to support HDMI.

A bit confusing!!!

Warm Regards,

Anil

0 Kudos

631 Views
sunithas
Contributor I

Hi Anil,

Could you add the HDMI monitor support for i.MX7 Sabre board? I am also facing display issue with i.MX7.

Please let me know, which display will work for i.MX7 Sabre board.

Regards,

Sunitha

0 Kudos