i want to use i.MX6ULL and bought the i.mx6ull-evk and installed Yocto ( from fsl-community-bsp)
but i coudn't find i.mx6ull configraution i just found imx6uevk configraution
and also downloaded L4.1.15_2.0.3_6ULL_patch_image but it isn't sources
could i build imx6ul-evk and use it ?
where could i get u-boot and kernel source of L4.1.15_2.0.36ULL ? and build in the yocto
thanks in advance
you can find all of the demo image you need for mx6ull evk from the link as below:
<MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP >.
pls focus on the "Board Support Packages"
if you need to build the source code for mx6ull evk, you can refer to the document named "i.MX Yocto Project User's Guide"
and you can download the document from the link as below:
thank you for the answer
i followed the doc ....and now in compiling ...
but if i downloaded the bsp from freescale.github.io ( 2.2-codname Morty )
there is no imx6ull machine configuration can i use imx6ul instead ?
thank you