AnsweredAssumed Answered

i.MX6 SPI-NOR boot.

Question asked by Anjalik Krishna on Aug 11, 2017
Latest reply on Aug 13, 2017 by Yuri Muhin
Branched from an earlier discussion

Hi Yuri,

  I am facing issue in SPI boot on i.MX6Q based Solo board.  When I boot image  from SD card and flash the u-boot binary to SPI flash ,  write is successful and able to read and erase the SPI NOR memory. But Uboot is not coming up once I change the boot media to SPI.

 

Below are the lines which I have used for SPI

EIM_D17 - MISO.alt1

EIM_D18 - MOSI.alt1

CSI0_DAT4 - CLOCK.alt2

EIM_EB2 - Chip Select

 

When we probed, the CS signal is appearing but no clock signals are coming. But the clock signals are being generated during read and write operations except during boot.

 

Can we use CSI0_DAT4 for clock instead of  EIM_D16.alt1? Is  EIM_D16.alt1 is mandatory for SPI NOR Boot?

Outcomes