AnsweredAssumed Answered

Re: i.MX6UL fuse prog for eMMC boot failed

Question asked by Andreas Wiesinger on Aug 8, 2017
Latest reply on Aug 10, 2017 by Yuri Muhin
Branched from an earlier discussion

Hi,

We tried it now with 

fuse prog 0 5 0x0000C86D

but it does not boot either. As we can workaround this by shortcutting a resistor on the board, we did not want to blow the 0x10 fuse as well, as this fuse will brick the board (and the workaround) completely.

 

My question is:  Is the fuse:

fuse prog 0 6 0x00000010

necessary to boot from the fuse settings or is it just a security setting? Currently, my only hope is, that this single fuse is necessary to "activate" the fuse settings from 0 5. If not, the settings we used for the second board (0x0000C86D) will not work either.

Can you help me out? Should I execute fuse prog 0 6 0x00000010 as well and risk bricking the second board fully?

 

Thanks!

Outcomes