AnsweredAssumed Answered

Target frequency of the core for i.MX6DL

Question asked by yuuki on Aug 9, 2017
Latest reply on Aug 11, 2017 by Artur Petukhov

Dear all,

 

The following is explained about Target frequency of the core in Reference Manual.

IMX6SDLRM Rev. 2, 04/2015
 1.4 Features (P.204)
====================================================================================
Target frequency of the core (including Neon and L1 cache) is 800 MHz non-overdrive
over the specified temperature range:
 . 1 GHz overdrive over the specified temperature range
 . 800 MHz non-overdrive over the specified temperature range
====================================================================================

 

Does MCIMX6U5EVM10** correspond to overdrive?

I think that this description is related only to MCIMX6U7CVM08**(Speed Grade: 800MHz).

 

May I have advice?

Best Regards,

 

Yuuki

Outcomes