ADC internal phase voltage channel gives 9 Volt once the battery voltage goes just beyond 18 Volt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC internal phase voltage channel gives 9 Volt once the battery voltage goes just beyond 18 Volt

375 Views
pratibhasurabhi
Contributor V

Hi,

I am implementing sensorless BEMF algorithm for BLDC motor.

I have used ADC internal channel for phase voltage.

When battery voltage is less than 18 Volt,channel shows minimum phase voltage but as we increase battery voltage beyond 18 Volts channel shows (battery voltage/2) as a phase voltage.

eg. If battery voltage is 17.9V then channel gives 300mV as a minimum phase voltage,

but If battery voltage is 18.2V then channel gives 9.1V as a phase voltage

Please tell is this behaviour is proper? If so what is the reason for this behaviour.

0 Kudos
1 Reply

242 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

 

That’s difficult to say.

The voltage depends on states of the FET transistors.

So if I understand, you don’t change the states with software/hardware, you only increase battery voltage and the states then change. Have you check error flags?

 

Regards,

Daniel

0 Kudos