PCI Express Controller Internal CSRs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCI Express Controller Internal CSRs

524 Views
michayardeny
Contributor III

In the manual P1022RM there is description of PCI Express Controller Internal CSRs at pci configuration 0x400 to 0x6FF .

Is there a public descriptions of that registers may it only be used for debug purpose. 

Micha

Labels (1)
0 Kudos
1 Reply

353 Views
ufedor
NXP Employee
NXP Employee

The implemented registers are described in the processor's RM starting from "16.11.16 LTSSM State Status Register (LTSSM_State_Status_Register)".

0 Kudos