AnsweredAssumed Answered

K64F + MCR20A border router commissioning app support

Question asked by Carlos Caloca on Aug 7, 2017

I have a K64F + MCR20A as a standalone border router, I already created the network with the "thr create" command, I seeing the BR sending advertissements with a sniffer application. However, I cannot see the BR appearing in the reference commissioning app (i'm using the Android version 1.01.02), the BR is connected to the Ethernet switch network via the K64F, the Ethernet and WIFI are interconnected to the office network.

 

Does the  K64F + MCR20 BR supports commissioning using the app? If the answer is no, Is there a NXP BR solution that does suppport the commissioning app? 

Outcomes