I am working on the eval board for S32K144x 100 pin package board. I looked at the schematic and it said that the potentiometer is connected to ADC0_SE12. However when i look at any example code the , especially the software triggered one, i find that the adc challel is listed as 11. Is there a GAP between the 2. I tried the software trigger code and the raw value changes according to the potentiomenter.
adc_chan_config_t adConv1_ChnConfig0 = {
.interruptEnable = false,
.channel = ADC_INPUTCHAN_AD11,
};
Am i missing something here?
Hi saurabhkarnik,
What SDK version are you using? I searched in latest versions and RTM , and see that the selected input channel is AD12, as would be expected.
Possibly this was an issue in earlier SDK versions, or a hardware change in EVB boards.
Still, getting valid raw data with AD11 is interesting. I will try to find if the potentiometer was indeed set to AD11 at some point.
I checked the firmware and seems we do change the value to 12 later. Maybe
the SDK needs to be udated or i am on previous version not sure. However it
works fine. My next question is if i want to trigger a software conversion
on 1st channel of ADC1 what would be the mask. Would it be channel 16+
assuming channels 0-15 are on ADC0 and 16+ are on ADC1 . Or would the ACDC
numbering restart from 0. I am particularly looking at the function below.
void convertAdcChan(uint16_t adcChan) { /* For SW trigger mode, SC1[0] is
used */
ADC0->SC1[0]&=~ADC_SC1_ADCH_MASK; /* Clear prior ADCH bits */
ADC0->SC1[0] = ADC_SC1_ADCH(adcChan); /* Initiate Conversion*/
}
Regards
Saurabh
On Thu, Aug 3, 2017 at 7:44 AM, ovidiualexandru <admin@community.nxp.com>
The numbering of ADC channels starts from 0 for each ADC instance. In the case above you would need to either have a new function that uses the ADC1 base address or to send the base address as a parameter to the function.
Regards,
Ovidiu