pixel clock drifts 10% on i.mx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pixel clock drifts 10% on i.mx6ul

581 Views
richard_hu
Contributor V

Hi,

I try to use a parallel LCD panel on i.mx6UL board.

And I  change the display timings to a standard VESA timings as the following:

============================================================

display0: display0 {
        bits-per-pixel = <32>;
        bus-width = <24>;
 
        display-timings {
            native-mode = <&timing0>;
            timing0: timing0 {
            clock-frequency = <40000000>;
            hactive = <800>;
            hfront-porch = <40>;
            hsync-len = <128>;
            hback-porch = <88>;
            vactive = <600>;
            vfront-porch = <1>;
            vsync-len = <4>;
            vback-porch = <23>;
            hsync-active = <0>;
            vsync-active = <0>;
            de-active = <1>;
            pixelclk-active = <0>;
            };
        };
    };

================================================================

Then I measure the signal of pixel clock on oscilloscope and get 36 MHz instead of 40 MHz.(It's about 10% errors.)

image002.jpg
Then I dump the clock tree information in kernel.

# mkdir -p /tmp/debug
# mount -t debugfs none /tmp/debug/
# cd /tmp/debug/clk
# cat clk_summary

================================================================

pll5_bypass_src                       1            1    24000000          0
       pll5                               1            1   651410064          0
          pll5_bypass                     1            1   651410064          0
             pll5_video                   1            1   651410064          0
                pll5_post_div             1            1   651410064          0
                   pll5_video_div           1            1   651410064
                      lcdif_pre_sel           1            1   651410064
                         lcdif_pred           1            1   108568344
                            lcdif_podf           1            1    36189448
                               lcdif_pix           1            1    36189448
                               iomuxc           0            0    36189448
                               lcdif_sel           0            0    36189448

================================================================
The "lcdif_pix" is about 36 MHz.

I also check the mxsfb.c

================================================================

static void mxsfb_enable_controller(struct fb_info *fb_info)
{
    ret = clk_set_rate(host->clk_pix,
    PICOS2KHZ(fb_info->var.pixclock) * 1000U);
}
static int mxsfb_restore_mode(struct mxsfb_info *host)
{
    vmode.pixclock = KHZ2PICOS(clk_get_rate(host->clk_pix) / 1000U);
    vmode.hsync_len = get_hsync_pulse_width(host, vdctrl2);
    vmode.left_margin = GET_HOR_WAIT_CNT(vdctrl3) - vmode.hsync_len;
    vmode.right_margin = VDCTRL2_GET_HSYNC_PERIOD(vdctrl2) - vmode.hsync_len -
    vmode.left_margin - vmode.xres;
}

================================================================

The clock frequency of "lcdif_pix" in clock tree is set by reference pixel clock (40 MHz).

Then get the pixel clock frequency from "lcdif_pix" (36 MHz).

I guess this problem results from the clock source(PLL) of pixel clock can't be set precisely.

Am i right ?

For some panels with critical timing, it may run into trouble.
Do you have any suggest to get rid of this problem?

Thank you !

Labels (2)
Tags (2)
0 Kudos
1 Reply

383 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

you are right, "lcdif_pix" is set by linux to possible closest value.

Since parent pll clock may be used by other peripherals so sometimes its

value can not be divided precisely for obtaining exact "lcdif_pix" value.

One can try to change parent pll or its value, if possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos