Hello All.
Im trying to use SB_loader.xex when i have 4 mx6 devices connected to usb and i want to load them im parallel.
I there a way to direct the SB_loader to a specific USB ? form my tries i noticed the he only load the first usb he encounter.
I didnt see any flag that i can set to direct it to a specific USB port.
BR,
Idan.
Hi Idan
I am afraid currently this is not supported, probably one can try to
modify application using sources
GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------