AnsweredAssumed Answered

powerpc cross-tool chain problem with SCons maker

Question asked by Ruonan Zhou on Jul 31, 2017
Latest reply on Aug 3, 2017 by ALEXANDER FEDOTOV

Hello,

I'm trying to write a SCons script to build my project, which was originally built in S32DS.

The project built fine with the Microsoft Visual C++ compiler. 

However, after specify the compiler PATH and the compiler powerpc-eabivle-gcc to use when building the project( that's the only environment setting I changed for the build), I got an error from powerpc-eabivle-gcc for every header file folder I include with CPPPATH, that there is no such file or directory.

 

I'm wondering if there's any special settings I need just for this compiler. Thanks for any suggestions/help:)

 

Ruonan  

Outcomes