AnsweredAssumed Answered

FRDM KW41Z  DATA TRANSFER

Question asked by Jalal Beladel on Jul 31, 2017
Latest reply on Aug 8, 2017 by Estephania Martinez Garcia

Hello,

 

I have coupled the two Transceivers FRDM KW41Z like the example on the nxp page ! I have a communication and if i press the Switch 4 or 3 of the one Transceiver lights up the LED of the other one Transceiver ( This is very good until now). Now when i ímport the LED example and debug it, lights up the LED only on one Transceiver and both Transceiver disconnected from the Ntetwork? i want only to run an application on one Transceiver an see it bei the other one! what can i do?

 

 

Thanks.

Outcomes