Is it possible to have the u-boot on a FAT32 partion?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to have the u-boot on a FAT32 partion?

1,562 Views
mzhang
Contributor I

Hi,

Here the current structure of the SD card we are using to boot the device:

1st partition: u-boot

2nd: boot

3rd: linux (root)

pastedImage_1.png

I'm wondering if it is possible to have something like this (a SD card for raspberry):

pastedImage_2.png

We'd like to be able to put a config file on a FAT32 boot partition which configures the device at boot.

This config file must be editable from a Windows machine.

The thing is Windows only "mount" the first partition of an "usb device", so it only see the 1st u-boot partition. (Windows 10 Creator Update allows to mount all the partitions, but from my test, it's not always working, and it doesn't recognize FAT12.)

Thanks.

MZ

Labels (3)
Tags (3)
0 Kudos
2 Replies

1,099 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 Kudos

1,099 Views
mzhang
Contributor I

MCIMX283CVM4B

0 Kudos