Hello friends,
I want to use the alarm timer to wake up from Deep-Sleep(LPC1830) . According to DataSheet,the Alarmtimer is connected directly to the 32kHz OSC. So my question is whether the 32kHz is external clock or internal clock? If it is a external clock should i connected a 32.768kHz Crystal oscillator to RTCX1/RTCX2 ?
I initialize the alarm timer like this:
LPC_CREG->CREG0 &= ~((1 << 3) | (1 << 2));
LPC_CREG->CREG0 |= (1 << 1) | (1 << 0);
LPC_ATIMER->DOWNCOUNTER = 2048;
LPC_ATIMER->PRESET = 1024;
but the DOWNCOUNTER doesn't count ·······
Solved! Go to Solution.
Hi,
Yes you need to connect an external 32.768kHz Crystal oscillator to RTCX1/RTCX2.
LPCOpen contains an example using alarm timer.
LPCOpen Software for LPC18XX|NXP
Have a great day,
Soledad
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Yes you need to connect an external 32.768kHz Crystal oscillator to RTCX1/RTCX2.
LPCOpen contains an example using alarm timer.
LPCOpen Software for LPC18XX|NXP
Have a great day,
Soledad
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you so much