Hi,
I am working on a project that consist in detecting the proximity of metallic containers through a plastic layer.
I am interested in the PCF8883 for its low power consumption.
Would it be possible to do that given the following details :
If not is there any other sensor that could do it?
Regards.
Hello Elyes,
NXP’s capacitive switches use a patented digital technique (patent from Edisen) to detect a change of capacitance on the device input. In order to use this switch, the following must first be defined:
A large distance (several meters) between the sensing plate and the IC is possible.
The circuit has three parameters that influence the switching behavior. Below they are listed in order of their influence:
I recommend using the PCF8883 evaluation board in order to evaluate the device.
I hope this information helps. Please let me know if you have any further question.
Regards,
David