The TAG from our customer works after ISO7816-4 (under ISO14443A-4, "Type 4 Tag Operation Specification") and the customer like to work with NDEF commands. Which reader can operate after these standard? Is it possible with PN7150 and 7120? Is the Sw for the Front Ends finished?
Dear Matthias Schwark, the PN7150|High Performance Plug'n Play NFC for OS|NXP would work this is a component that is full NFC compliant also PN7150 embeds a new generation RF contactless front-end supporting various
transmission modes according to NFCIP-1 and NFCIP-2, ISO/IEC14443, ISO/IEC 15693,
MIFARE and FeliCa specifications.
Have a great day !!
BR
Jonathan