AnsweredAssumed Answered

T2080 Routing

Question asked by Matias Lirman on Jul 26, 2017
Latest reply on Aug 20, 2017 by Yiping Wang

Hello,

 

I have been working with the T2080RDB board and am trying to configure a bridge between two disconnected networks

 

 

After enabling the board I successfully create a bridge with the following commands:

 

brctl addbr br0

brctl addif br0 fm1-mac10 fm1-mac3

ip link set fm1-mac10 up

ip link set fm1-mac3 up

ip link set br0 up

ip addr add 192.168.1.60/24 brd + dev br0

 

I now have full communication between the device connected through fm1-mac10 and fm1-mac3. I am trying to initialize this bridge un boot up automatically. I have been editing the /etc/network/interfaces file, which looks like so:

 

# The loopback interface
auto lo
iface lo inet loopback

 

auto br0
iface br0 inet static
address 192.168.1.60
netmask 255.255.255.0
bridge_ports fm1-mac3 fm1-mac10
bridge_stp off
bridge_fd 0
bridge_maxwait 0

 

This should, by everything ive researched online, initialize a bridge on boot up but it has not been successful thus far. I tried adding the following lines to the /etc/network/interfaces file to see if anything changed but everything remained the same on boot up:

 

auto fm1-mac10
iface fm1-mac10 inet manual

 

auto fm1-mac3
iface fm1-mac3 inet manual

 

Any help on this matter would be much appreciated as I do not know what else to try

 

Thanks in advance!

 

Best,

Matias Lirman 

 

Outcomes