Rupert C

LPC-link 2 + windows 10 driver problems

Discussion created by Rupert C on Jul 27, 2017
Latest reply on Jul 27, 2017 by LPCX presso support

I'm running Windows 10 in VirtualBox on Mac OSX.

 

With LPC Xpresso cannot connect to LPC link 2.

 

Looking in the Windows 10 "Devices and Printers" control panel there is a warning sign on the LPC Link 2 icon which leads to information as below.

 

All the drivers and sofware versions are the latest and have restarted.

 

Any suggestions please?

 

Device USB\VID_1FC9&PID_0090\JQD4FXOT had a problem starting.

Driver Name: usb.inf
Class Guid: {36fc9e60-c465-11cf-8056-444553540000}
Service: usbccgp
Lower Filters:
Upper Filters:
Problem: 0xA
Problem Status: 0xC000000D

 

(Windows 10 Screenshot attached too.)

Attachments

Outcomes