I am using MQX example of USB host CDC serial communication.
I am able to enumerate the CP2102 board and it is in resume state.
But I am not able to send command on it.
Like when I want to send the set descriptor command to it ( Interface descriptor) it is not giving me the same value when I do the get descriptor.
I am using K22FN512 on a FRDM board as USB host. Kindly support to get these two boards get communicated.
Thanks and Regards,
Jatin Vashisth
I assuem you are using MQX 4.1, to get the USB host cdc work,several steps needs to be done.
Please refer to the below link to see whether it helps
https://community.nxp.com/docs/DOC-101456
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------