AnsweredAssumed Answered

How to flash S32 project for MPC564xL using Rappid bootloader?

Question asked by deepak313 on Jul 24, 2017
Latest reply on Jul 25, 2017 by deepak313

I created a project for MPC5643L in S32 design studio v1.2 and built and created a .srec file.

I do not want to use JTAG to flash.

Using Rappid bootloader utility, I can flash this .srec using serial port, but the code does not seem to run.

(I have another .mot file that I can flash using serial port and Rappid and it runs, so I am sure that the hardware and Rappid connection/configuration are okay).

I believe the .srec file may be missing some information.

How can I configure S32 options to generate a .srec to be able to flash using Rappid bootloader?

Outcomes