LPC54608 RS485 example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 RS485 example

2,021 Views
rolandhösch
Contributor I

Is there any example out there who to configure a flexcomm USART port of the LPC54608 for serial RS485 communication?

Labels (1)
Tags (1)
2 Replies

1,004 Views
primate
Contributor III

Opening the thread again since I am planning to get the LPCXpresso54628 Development Board but I am not sure how to implement the RS485 protocol entierly.

Also, I found an example RS485 and I presume the code can be modified to fit into the LPCXpresso54628 

Two LPC1765 devices communicating through RS-485? 

Thank for any help.

0 Kudos

1,004 Views
soledad
NXP Employee
NXP Employee

Hi,

We only have the SDK for LPC54608 examples.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos