About board stucking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About board stucking

518 Views
samikshadubey
Contributor I

Hi All,

I am working on imx6sl sololite processor. My board was working fine but suddenly when i load the new images it stuck with these logs.

VFS: Cannot open root device "ram" or unknown-block(1,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 1024 mtdblock0 (driver?)
1f01 13312 mtdblock1 (driver?)
1f02 2048 mtdblock2 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
[<80040518>] (unwind_backtrace+0x0/0xf8) from [<804145d4>] (panic+0x74/0x188)
[<804145d4>] (panic+0x74/0x188) from [<80008d58>] (mount_block_root+0x170/0x224)
[<80008d58>] (mount_block_root+0x170/0x224) from [<80008ef4>] (mount_root+0xe8/0x108)
[<80008ef4>] (mount_root+0xe8/0x108) from [<80009040>] (prepare_namespace+0x12c/0x184)
[<80009040>] (prepare_namespace+0x12c/0x184) from [<80008a24>] (kernel_init+0xf4/0x124)
[<80008a24>] (kernel_init+0xf4/0x124) from [<8003b670>] (kernel_thread_exit+0x0/0x8)

And i did not remember where i had change in sdk so that it gives above.

Can anyone Please help me out.

0 Kudos
1 Reply

407 Views
igorpadykov
NXP Employee
NXP Employee

Hi samiksha

please run ddr test

https://community.freescale.com/docs/DOC-105652 

and rebuild image with new calibration coefficients found from test.

Probably new images were for other board (like nxp reference board)

or had incorrect kernel boot parameters. One can check it in documentation

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos