Hi Guys,
I download the dual motor control project from NXP :http://www.nxp.com/downloads/en/apps/MTRCKTDPS5643L_SW.exe ,and i import the project into S32 V1.1,i compile it there is no errror,but when i debug it into the board ,there some error shown as below:
and the code don't download into the MPC5643L.
How to solve it ?
the Attachment is the Project
Original Attachment has been moved to: Test_9.zip
Hi,
I have loaded your code into micro flash with Lauterbach debugger without any issues.
However code reports FCCU errors and after execution micro goes into safe state.
So you should check your debugger settings and loading script as your issue is there.
Peter