license authorizaton

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

license authorizaton

601 Views
assangeye
Contributor I

捕获.JPG

when i install the software completely ,finding license authorizaton ,it tells me there is a err.Now my code is over 32K and  i have a license,but i can't use it .how can  do it?

0 Kudos
1 Reply

372 Views
TomasPaez
NXP Employee
NXP Employee

License file needs to be placed in the following directory,

You can discard the help menu option for license authorization. 

Just locate a valid license file in the following directory C:\Program Files (x86)\Freescale\CWS12v5.1

Make sure you have admin access so you can write in program files directory, if not check with the local admin to get this.

hope this helps  

0 Kudos