The S9S08RNA16W2MLCR A2D data sheet specifies the range of input pin leakage currents as -1uA to +1uA. I have high impedance series input resistors (500Kohm to 1MHom) to a pair of analog signals the connect to two microcontroller A2D input pins. Can I assume that the leakage currents of the two A2D input pins will match if the input voltage are the same? That is, if one pin leaks 1uA , will the other pin leak 1uA as well if both input voltage are the same?